Feedback_Calibration_Current
| Index.Sub | 2230.1CH |
| Data Type | Unsigned16 |
| Access | Read/Write |
| PDO Mappable |
No |
| Unit |
milliamperes (mA) |
|
Range |
0 to Motor max current |
| Default Value | 100 |
| Store Supported | Yes |
| Description | This value is used for Closed Loop feature and defines motor current value used during the Feedback Calibration procedure. |
|
Notes |
(1) available with firmware V00r75 or superior. |